S32K344 - Wake up on can message

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 - Wake up on can message

Jump to solution
439 Views
RBSamuel
Contributor III

Hello everyone!

I need to create a code for the S32K344 microcontroller that should wake the MCU up when receive a specific can message. Is there any example or tip to implement this?

I saw on the following topic that I can't use the FlexCAN module directly.

Solved: S32K3 Wake up method - NXP Community

Then I configured the CAN0 TX/RX and also set the RX to be WKUP, but nothing happens after MCU enters in standby.

RBSamuel_0-1709643871074.png
For this specific wkpu, I'm trying to use the wkpu module for the hardware interrupt 19, according to the S32K3xx_IOMUX.xlsx.


Thank you.

 

Tags (3)
0 Kudos
Reply
1 Solution
430 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @RBSamuel,

You can use the following application note as base, which showcases various wakeup use cases, including FlexCAN: S32K3 Low Power Management AN and demos - NXP Community

Best regards,
Julián

View solution in original post

1 Reply
431 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @RBSamuel,

You can use the following application note as base, which showcases various wakeup use cases, including FlexCAN: S32K3 Low Power Management AN and demos - NXP Community

Best regards,
Julián