S32K344 SAF FCCU Fault Injection never returns

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 SAF FCCU Fault Injection never returns

Jump to solution
337 Views
lluo
Contributor III

Hi,

I am currently working with s32 saf demo. I got the demo after installing the S32 SAF framework version S32K3_SAF_1.0.4_EVAL_D2312. 

lluo_1-1709890721934.png

During running the demo, I found out when I tried to inject the following fault:

eMcem_InjectFault( EMCEM_DCM_NCF_1_AD_EDC_ERR_OUT )

the function never returned. After a detailed look,I found out that the program got stuck in the following place:

lluo_2-1709890862102.png

It failed writing to the register.

Do you probably have any idea about why this happened? Thank you in advance. 

 

 

 

0 Kudos
Reply
1 Solution
306 Views
lluo
Contributor III

The issue is solved by the following configuration:

lluo_0-1710210406292.png

In the Reaction Type section, select "No reset reaction" instead of "Short reset reaction".

The issue can be closed.

 

View solution in original post

Tags (1)
0 Kudos
Reply
1 Reply
307 Views
lluo
Contributor III

The issue is solved by the following configuration:

lluo_0-1710210406292.png

In the Reaction Type section, select "No reset reaction" instead of "Short reset reaction".

The issue can be closed.

 

Tags (1)
0 Kudos
Reply