S32K324 HSE固件如何安装?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K324 HSE固件如何安装?

Jump to solution
392 Views
cx9
Contributor I

我正在开发S32K324,S32K324哪里可以找到安装HSE固件的软件工程?

0 Kudos
Reply
1 Solution
368 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please downloaded from S32K3 Standard Software > Automotive SW - S32K3 - HSE Firmware >  S32K344 HSE FW 0.2.40.0 SR Release. Note: This release supports the S32K344, S32K324, and S32K314. The HSE_DEMOAPP_S32K3XX_0_2_40_0.exe can be found in S32K311 HSE FW 0.2.40.0 RTM Release.

If you don't have the Lauderbach and only have the PEMicro or J-Link debugger, then please download S32K3_HSE_DemoExamples. It is recommended to refer to the discussion in HSE firmware installation.

Due to limited resources, we are currently unable to support customers writing from generic email accounts such as gmail.com or qq.com or similar. Please ensure that you use your company email address when communicating with NXP so that we can prioritize your question accordingly. Thank you for your understanding.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
369 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please downloaded from S32K3 Standard Software > Automotive SW - S32K3 - HSE Firmware >  S32K344 HSE FW 0.2.40.0 SR Release. Note: This release supports the S32K344, S32K324, and S32K314. The HSE_DEMOAPP_S32K3XX_0_2_40_0.exe can be found in S32K311 HSE FW 0.2.40.0 RTM Release.

If you don't have the Lauderbach and only have the PEMicro or J-Link debugger, then please download S32K3_HSE_DemoExamples. It is recommended to refer to the discussion in HSE firmware installation.

Due to limited resources, we are currently unable to support customers writing from generic email accounts such as gmail.com or qq.com or similar. Please ensure that you use your company email address when communicating with NXP so that we can prioritize your question accordingly. Thank you for your understanding.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
294 Views
cx9
Contributor I
Thank you very much for your answer.
0 Kudos
Reply