Hi,
Thank you so much for your interest in our products and for using our community.
There is no demo but you can perform duty-cycle and period transitions during runtime with OPWFMB mode. You can refer to the 63.5.3.16 Output Pulse Width and Frequency Modulation Buffered (OPWFMB) mode section from reference manual.
Hope it helps you.
Have a nice day!
Hi, Leo
Thanks for you kind reply, and I know the OPWFMB mode, it is triggered by internal counter. If I want to use two or more channels to output different PWM, since the internal counter can not be started at the same time point, so how can I sychronize these PWM?
hi, leo
we use EB tresos to do the MCAL development right now, and each PWM channel has its own internal counter, so we can not set one of them as the time base for another PWM channel. then, we try to change the MCAL plugin static code, and Enable the Output Update for Channels in sequence, since each invoke can not be started at the same time, so the each PWM channel phase will deviate some nanoseconds. but I don't think it is the perfect solution, so I want to know how could you achieve? if possible, could you please give me the demo? thanks in advance.
We do not have the demo that you request, but you can refer to 4.2.3.1. eMIOS section from AN13884 or AN13767 to see how one eMIOS channel (in MCB mode) is configured as a time base for PWM signals (in OPWMB mode).