S32K324 Emios pwm output with dynamic frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K324 Emios pwm output with dynamic frequency

271 Views
witness
Contributor III

hi, experts

Does NXP S32K324 support PWM output with variable frequency? that means when software running, we can be able to adjust frequency dynamically. 

0 Kudos
Reply
6 Replies

236 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

There is no demo but you can perform duty-cycle and period transitions during runtime with OPWFMB mode. You can refer to the 63.5.3.16 Output Pulse Width and Frequency Modulation Buffered (OPWFMB) mode section from reference manual.

Hope it helps you.

Have a nice day!

0 Kudos
Reply

227 Views
witness
Contributor III

Hi, Leo

Thanks for you kind reply, and I know the OPWFMB mode, it is triggered by internal counter. If I want to use two or more channels to output different PWM, since the internal counter can not be started at the same time point, so how can I sychronize these PWM?

0 Kudos
Reply

201 Views
_Leo_
NXP TechSupport
NXP TechSupport

You can use one channel as time base for the others channels. Then use AS1 and BS1 registers to change duty cycle and period, respectively of the channels configured as OPWFMB mode.

0 Kudos
Reply

172 Views
witness
Contributor III

hi, leo

we use EB tresos to do the MCAL development right now, and each PWM channel has its own internal counter, so we can not set one of them as the time base for another PWM channel. then, we try to change the MCAL plugin static code, and Enable the Output Update for Channels in sequence, since each invoke can not be started at the same time, so the each PWM channel phase will deviate some nanoseconds. but I don't think it is the perfect solution, so I want to know how could you achieve? if possible, could you please give me the demo? thanks in advance.

 

0 Kudos
Reply

162 Views
_Leo_
NXP TechSupport
NXP TechSupport

We do not have the demo that you request, but you can refer to 4.2.3.1. eMIOS section from AN13884 or AN13767 to see how one eMIOS channel (in MCB mode) is configured as a time base for PWM signals (in OPWMB mode).

0 Kudos
Reply

140 Views
witness
Contributor III

I have looked through the reference manual, but did not find the info you mentioned, can you send me yours or send me the link that I can be able to download.

0 Kudos
Reply