Hello.
When I send data to MOSI by called Spi_SyncTansmit(), SCK and MOSI make wrong pulse at start.
It happen only in use CPOL=1(Clock Idle HIGH, Active LOW).
If I set CPOL=0 (Clock Idle Low, Active HIGH), it is okay.
* RTD Version 2.0.1 (7, July, 2022)
1. Send 0x00 00
2. Send 0x07 31
3. LPSPI_1 Register value
Best Regards,
Sean Sung
已解决! 转到解答。
Dear @ssean,
The issue is that the Lpspi_Ip_SyncTransmit() resets the LPSPI module in function Lpspi_TransmitTxInit().
You would need to remove the code that reset the LPSPI from the function.
Regards,
Daniel
Hi @ssean,
It was discussed here:
https://community.nxp.com/t5/S32K/S32K3-SPI-CS-problem-when-using-GPIO-to-simulate-CS/td-p/1564367
The module is reset at the beginning of each transfer.
Normally, with your configuration OUTCFG = 0, the MOSI line should retains last value when chip select is negated (beetween transfers).
But the module is reset in the driver.
Regards,
Daniel
Dear @ssean,
The issue is that the Lpspi_Ip_SyncTransmit() resets the LPSPI module in function Lpspi_TransmitTxInit().
You would need to remove the code that reset the LPSPI from the function.
Regards,
Daniel