Hello
I saw in the S32K3xx Low Power Management.pdf that there is such a description in the [6.3. VLSR mode entry] chapter [FIRC must be divided by 16 to provides a 3 MHz clock source for the core, the bus, the peripheral clocks and flash memory access mode (750 KHz).].
I use the DS tool to configure a clock tree different from RUN Mode, which uses FIRC as the clock source, but the FIRC clock cannot be divided by 16 to assign to CORE_CLK, and the value of clock division is at most 8.
How to divide FIRC into 16 when entering StangBy?
BestRegards
解決済! 解決策の投稿を見る。
Hi, could you give me reference to S32K3xx Low Power Management.pdf?
Following register allows to setup FIRC divided by 16:
Thanks for your answer, can you please tell me how to configure this register using DS tool?
BestRegards
Click on Fast RC, an on the right side you may choose a frequency.