S32K312 ADC Channel mapping

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 ADC Channel mapping

188 Views
sungjun
Contributor II

hello? NXP Team
I am currently using S32 Design Studio for S32 Platform 3.4.
The MCU is S32K312, and I am curious about how to set up the ADC channel.

To set up the ADC in S32 Design Studio for ARM Version 2.2,
Just set the Input Channel according to the Name in the Configuration list as shown below.

sungjun_2-1712912558038.png

What screens can I refer to in S32 Design Studio for S32 Platform 3.4?

And what information in S32K3xx_RM should ext_in refer to in the ADC setting signal?

sungjun_1-1712912467439.png

sungjun_3-1712912684024.png

Lastly, I would like to know the meaning of ADC0_X[0] and ADC0_MA[2:0] = 3'h0 in the picture below.

It's a hassle, but please explain in detail.

sungjun_4-1712912747882.png

Thank u!

 

 

0 Kudos
1 Reply

163 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @sungjun 

What screens can I refer to in S32 Design Studio for S32 Platform 3.4?

We recommend using the newest S32DS version (3.5) with the latest S32K3 software (RTD 4.0.0) releases. To understand how the ADC can be configured with ConfigTools please use the examples provided with the RTDs. 

And what information in S32K3xx_RM should ext_in refer to in the ADC setting signal?

This pin corresponds to the ADC1_X[1]. You can consult the assignment in the S32K312_IOMUX attached to the S32Ke reference manual. 

Meaning of ADC0_X[0] and ADC0_MA[2:0] = 3'h0. 

Check the following community thread. It has information related to the topic.

S32K3 ADC Use of external channels

 

B.R.

VaneB

 

0 Kudos