S32K3 frequency measurement on FLEXio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 frequency measurement on FLEXio

ソリューションへジャンプ
397件の閲覧回数
Tobias12
Contributor I

Hi all,

I am looking for a possibility to measure frequencies on the S32K FLEXios. Unfortunately EMIOS has not enough channels for my application.

The goal is to measure frequencies up to 20kHz.

Is it possible to use the FLEXios or is there another option I don't see?

 

Thanks

Tobias 

0 件の賞賛
返信
1 解決策
373件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Tobias,

There are just EMIOs and the FlexIO for HW input capture.

The FlexIO input capture is used in emulated SENT receiver (RM, 73.6.8 SENT receiver).

There are SENT receiver examples in RTD, so you can refer to that.

 

Regards,

Daniel

 

元の投稿で解決策を見る

1 返信
374件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Tobias,

There are just EMIOs and the FlexIO for HW input capture.

The FlexIO input capture is used in emulated SENT receiver (RM, 73.6.8 SENT receiver).

There are SENT receiver examples in RTD, so you can refer to that.

 

Regards,

Daniel