S32K3 RTD for EIM and ERM peripherals

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 RTD for EIM and ERM peripherals

ソリューションへジャンプ
1,605件の閲覧回数
ziomocci
Contributor IV

 

Hi all,

 We are working on ECC error handling (both in SRAM and in FLASH) for the S32K344 device, but I have not found the relative Ip Driver on RTD version 4.4.2.0.0 D2203.

I have seen that a few SDK examples are proposed for different devices (S32K31..).

ziomocci_0-1671032057403.png

 

ziomocci_1-1671032113381.png

 

Could we use these samples, with a few modifications if needed, with a S32K344 device?

K.R

Andrea

 

0 件の賞賛
返信
1 解決策
1,481件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @ziomocci 

All .zip files can be installed this way.

VaneB_0-1673299110672.png

VaneB_1-1673299153075.png

VaneB_4-1673299342767.png

VaneB_5-1673299408671.png

Could you please validate if the following works for you?

 

B.R.

VaneB

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
1,585件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @ziomocci 

There is not an specific Ip Driver on RTD for the ECC.

In the S32K1 the ECC errors are handled automatically by the EEE state machine. In S32K3, it has not HW state machine based EEE as the K1.
I suggest you to take a look to the these application notes:

S32K1 to S32K3 Migration Guidelines 

S32K3 Memories Guide 

Also, take a look to the User Manual for S32K3 FEE Driver included in the RTD.

 

B.R.

VaneB

0 件の賞賛
返信
1,574件の閲覧回数
ziomocci
Contributor IV

Hi @VaneB,

 I have found an S32K144 and tried both demo Applications from NXP, that is

erm_report_s32k144,

eim_injection_s32k144.

for observing the correct behaviors of EIM/ERM, but in both cases S32DS debugger stops here

ziomocci_0-1671554781869.png

 

Sencondly, I was trying to repeat the test with an S32K3 (configurations Word0/1 of EIM channels 0/1 are the same for both) w/o success.

So, is there a way to test those functionalities of injection and reporting?

It could be a safety problem for the controller.

B.R.

Andrea  

0 件の賞賛
返信
1,562件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

I suggest you to take a look to the S32 Safety Software Framework (SAF) and Safety Peripheral Drivers (SPD) for the S32K3.

I hope this will help you.

0 件の賞賛
返信
1,490件の閲覧回数
ziomocci
Contributor IV

Hi @VaneB ,

I have download the archives form NXP site, unzipped and installed following instructions listed in S32K3_SAF_1.0.1_EVAL_ReleaseNotes.txt file but an error appear in S32DS 

ziomocci_0-1673262370765.png

Could youi help me for eMCEM IP driver installation?

0 件の賞賛
返信
1,482件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @ziomocci 

All .zip files can be installed this way.

VaneB_0-1673299110672.png

VaneB_1-1673299153075.png

VaneB_4-1673299342767.png

VaneB_5-1673299408671.png

Could you please validate if the following works for you?

 

B.R.

VaneB

 

 

0 件の賞賛
返信
1,462件の閲覧回数
ziomocci
Contributor IV

Hi @VaneB,

 I have solved the installation issue with the NXP internal support.

Now I am able to install the SAF EVAL version for the S32K344.

Thank you very much.

Regards,

Andrea

0 件の賞賛
返信
1,476件の閲覧回数
ziomocci
Contributor IV

Hi @VaneB ,

Your guide line does not work properly in my case.

First, I see only one package

ziomocci_0-1673336451368.png

whereas you are able to check two packages for installation.

Second, after clicking the "Next" button, 

ziomocci_1-1673336530506.png

 

At the moment the problem is unresolved. Could be better to open a Support Request to NXP Technical Support?

 

B.R.

Andrea 

0 件の賞賛
返信