S32K148EVB - Not able to connect, Reset LED always on

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K148EVB - Not able to connect, Reset LED always on

590 次查看
luk90as
NXP Employee
NXP Employee

I am not able to connect to the S32K148 board via OpenSDA USB using S32DS v2.2 for ARM. The Board shows on the explorer and also on the device manager. The used port is automatically recognized in the debug configuration in S32DS. The Reset LED D11 is always on. 

I tried to recover the board using kinetis Recovery Utility, but it was unable to halt the processor. I used the OpenSDA interface via USB.

0 项奖励
回复
2 回复数

393 次查看
eshivashankar
Contributor I

same issue for me also...D11 is always on...

 

0 项奖励
回复

581 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Lukas,

What error message do you get from the debugger?

 

BR, Daniel

0 项奖励
回复