Hi All,
I use S32K148 and SDK 4.0.3 to control other SPI slaves.
Below is the data transferred with SPI.
Ch0 : SPI CS
Ch1 : SPI MISO
Ch2 : SPI MOSI
CH3 : CLOCK
CH4 : For debugging, I/O toggles before SPI doing transferred
In the normal mode, Ch4 toggled before the SPI transferred data.
In some cases, the SPI transfers one more data after the correct data transferred, but the toggle pin does not toggle before.
After that, SPI is stalled and doesn't transfers data again.
Also, the SPI Status is keeping in busy mode.
How could I do to fixing this issue to make SPI working normally?
Leon
Solved! Go to Solution.
You can change it to SAMPLE = 0.
This loopback feature (SAMPLE = 1) is implemented on LPSPI0 and on PTD15 and PTE0 only.
The CFGR1[1] SAMPLE bit improves the setup time of the input data from the slave (MISO signal).
Becasue if SAMPLE = 1 the Master does not sample the internal SCK signal but the actual SCK signal on the bus.
This is useful at higher baudrates.
tSU: Data setup time(inputs) is specified in the DS, Table 46. LPSPI electrical specifications (NUM 6).
tSU min 29ns (SAMPLE = 0, at 5V, RUN)
tSU min 7ns (SAMPLE = 1, at 5V, RUN)
Regards,
Daniel
Hi @Leon06,
Do you use interrupt or DMA mode?
Is there any error feedback event, or do the APIs return any error status codes?
Can you share the project so that I can test it on my side?
Regards,
Daniel
Hi Daniel,
I use the the SPI configuration as below setting.
/*! @brief SPI_PAL instance */
spi_instance_t spi1Instance =
{
.instType = SPI_INST_TYPE_LPSPI,
.instIdx = 1U
};
/* SPI Master Configurations */
spi_master_t MasterConfig0 =
{
.baudRate = 250000U,
.ssPolarity = SPI_ACTIVE_LOW,
.frameSize = 16U,
.clockPhase = READ_ON_EVEN_EDGE,
.clockPolarity = SPI_ACTIVE_LOW,
.bitOrder = SPI_TRANSFER_MSB_FIRST,
.transferType = SPI_USING_DMA,
.rxDMAChannel = 0U,
.txDMAChannel = 1U,
.callback = NULL,
.callbackParam = NULL,
.ssPin = 3,
.extension = NULL
};
Once the fault exits, the bit24 of the SPI SR (Status Register) is 1, indicating that the SPI channel is keeping in busy status.
I am using the DMA triggered by LPIT every 2ms about SPI Tx data.
Leon
HI Leon,
Since the GPIO stops toggling, it must be stuck somewhere.
Do you see any DMA error?
If you don't want to share the project here, you can create a ticket.
Regards,
Daniel
Hi Daniel,
These days, I continued working on solving this case.
I checked the dma status, no error occured.
I found if there are some noises on the SPI clock, it could easily make the SPI transferred error.
Below is the SPI signal monitored by the logic analyzer. I have noticed a 2ns clock noise on the SPI clock signal, which could potentially cause errors during data transfer.
If the clock noise continuously exists, the SPI error would easily occur.
I'm still confused as to why the SPI successfully transfers the data frame, the CS pin returns to high, but then the CS pin goes low again and the transfer of another data frame fails, resulting in the SPI channel being stalled. It's quite strange.
I'm sorry for I couldn't share the project because of our company's policy.
How could I share the enough informations for solving this case?
Thanks.
Leon
Hi @Leon06,
Regarding the noise on the SCK line, it can impact the transceiver if CFGR1[SAMPLE] = 1.
Otherwise the LPSPI sees the internal SCK signal only.
Is SAMPLE set in the project?
Thanks,
BR, Daniel
Hi Daniel,
Below is the SPI channel register.
What should I set this register?
Regards,
Leon
Can you try with 0x0000_0001?
Thank you
Hi @danielmartynek ,
Thanks for your suggestion, I changed the value to CFGR1[SAMPLE] = 0x0000 0001.
For now, it's working.
But I check the SDK 4.0.3 lpspi_master_driver.c, the function
status_t LPSPI_DRV_MasterConfigureBus(uint32_t instance,const lpspi_master_config_t * spiConfig,
uint32_t * calculatedBaudRate) is always setting the CFGR1 Bit1 = true.
So should I change line374 to LPSPI_SetSamplingPoint(base, false);? If I make this change, will it cause any other proplems?
Regards,
Leon
You can change it to SAMPLE = 0.
This loopback feature (SAMPLE = 1) is implemented on LPSPI0 and on PTD15 and PTE0 only.
The CFGR1[1] SAMPLE bit improves the setup time of the input data from the slave (MISO signal).
Becasue if SAMPLE = 1 the Master does not sample the internal SCK signal but the actual SCK signal on the bus.
This is useful at higher baudrates.
tSU: Data setup time(inputs) is specified in the DS, Table 46. LPSPI electrical specifications (NUM 6).
tSU min 29ns (SAMPLE = 0, at 5V, RUN)
tSU min 7ns (SAMPLE = 1, at 5V, RUN)
Regards,
Daniel