[S32K148] No CLKOUT from SOSC_DIV2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[S32K148] No CLKOUT from SOSC_DIV2

1,032 次查看
114454338
Contributor I

My setup is not using SDK, but AutoSar package instead.

Now, I want to use CLKOUT pin(PTE-10) to monitor SOSC_DIV2 frequency, but failed.

(If monitor other clock outputs(FIRC, SIRC...), all are no problem, only SOSC, no output generated!)

My SCG registers setting shows below:

2019-10-22_090439.png

SIM registers setting as below:

2019-10-22_090334.png

So, from the Clocking diagram in S32K1xx user manual, I didn't find any mistake.

Could someone support me about this issue? Is there any other configuration I need to check?

2019-10-22_085508.png

Thank you.

0 项奖励
回复
2 回复数

956 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

I'm using S32K148EVB. I tried to set the same clock settings as you and I can measure the SOSCDIV_2 on PTE10 pin without any problem. I attached the simple test code. Please, could you try it on your side?

I hope it helps.

Best Regards,

Diana

0 项奖励
回复

956 次查看
114454338
Contributor I

Hello, Diana, 

I appreciate for your kindly support and I would like to try it as soon as possible,

but unfortunately I'm facing another show stopper issue mentioned by another question. "https://community.nxp.com/thread/515788"

My EVB cannot flash and debug since yesterday... 

Could you kindly give me some support how could I fix it first?

Thanks a lot

0 项奖励
回复