In the OpenSDA_Release_Notes.txt from the latest PEMicro applications zip, I see the following:
MSD - DEBUG version 1.21
- added new board support for S32K142EVB-Q100
- added new board support for S32K146EVB-Q144
- added new board support for S32K148EVB-Q144
Which firmware file do I program on the S32K146EVB-Q144 to do debugging via OpenSDA? I see a MSD-DEBUG-EVB-S32K144_Pemicro_v119.SDA and a MSD-DEBUG-S32K142EVB-Q100_Pemicro_121.SDA.
I tried the MSD-DEBUG-S32K142EVB-Q100_Pemicro_121.SDA. When the board boots I see an "S32K142EVB" mass storage device. The D2 LED is solid green and the D11 LED is flashing red continuously.
Also, I have an "OpenSDA - CDC Serial Port" device in the Windows device manager, but when I connect to that COM port I don't see any messages. I'm using baud rate 115200. Should I see any debug port messages when I reset the evaluation board?
Versions in my SDA_INFO.HTM file: <form id="form1" name="form1" method="post" action="http://www.pemicro.com/opensda/index.cfm">; <input name="tag" type="hidden" id="tag" value="description" /> <input name="BOARD" type="hidden" id="BOARD" value="S32K146EVB-Q144" /> <input name="BOOTVER" type="hidden" id="BOOTVER" value="1.11" /> <input name="APPVER" type="hidden" id="APPVER" value="1.21" /> <input name="DUID" type="hidden" id="DUID" value="CF333938-0B3581D5-375AC80F-D349E678" /> <input name="EUID" type="hidden" id="EUID" value="C7B1A239-A2178737-1859AA14-F95268D6" /> <input name="TUID" type="hidden" id="TUID" value="74823938-47328196-8467AE18-C23B9871" /> <!--476--> <input name="TOA" type="hidden" id="TOA" value="86B6E505-7F935864-79B2A114-1E5AB1C6" /> <input name="TOA2" type="hidden" id="TOA2" value="86B6E505-BF15C9AA-AF6E54B6-0D356245" /> <input name="SUID" type="hidden" id="SUID" value="86B6E505-5BA18877-37239804-8003EC65" /> <input name="MICROVER" type="hidden" id="MICROVER" value="1.08" /> <input name="APPNAME" type="hidden" id="APPNAME" value="PEMicro S32K142EVB-Q100 Mass Storage/Debug App" />
Hi,
I have difficulties to understand this request.
The board comes with pre-installed drivers, you can connect it to PC and use S32 Design Studio IDE.
Do you have a problem to use it in Design Studio?
The OpenSDA emulates UART, but there will be nothing on the terminal unless the S32K is programmed with an application that use UART.
Regards,
Daniel