S32K146EVB Board LPI2C unable to Test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K146EVB Board LPI2C unable to Test

Jump to solution
1,400 Views
Nibesh
Contributor III

Hello @VaneB I am unable to test LPI2C Example code.
I have checked the datasheet, the PTA2 and PTA3 pin is not connected (DNP).
So do I have to short with 0ohms Resistor. 

0 Kudos
Reply
1 Solution
1,376 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Nibesh 

Some hardware changes are required to run the LPI2C SLAVE/MASTER example. 

R146 (PTC0) and R147(PTA6) are placed by default, remove and place R544 (PTE11) and R543 (PTE10) for I2C functionality with FLEXIO or R542 (PTA2) and R541 (PTA3) for LPI2C. Also, it is mentioned in the examples documentation that two pull-up resistors should be connected, one between VCC(J3.7) and SDA pin(J1.1) and the second one between VCC(J3.7) and SCL pin(J1.4).

Please make the HW changes according to any of the mentioned options.

Note: the first HW recommendations are based on the following schematic: S32K146EVB-Q144 Evaluation Board Schematics.

View solution in original post

3 Replies
1,385 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Nibesh 

Which software are you using (SDK or RTDs)? 

 

B.R.

VaneB

0 Kudos
Reply
1,381 Views
Nibesh
Contributor III

Hello @VaneB 
I am testing both RTM and S32DS Example Code.
I am using S32Design Studio IDE for it..

0 Kudos
Reply
1,377 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Nibesh 

Some hardware changes are required to run the LPI2C SLAVE/MASTER example. 

R146 (PTC0) and R147(PTA6) are placed by default, remove and place R544 (PTE11) and R543 (PTE10) for I2C functionality with FLEXIO or R542 (PTA2) and R541 (PTA3) for LPI2C. Also, it is mentioned in the examples documentation that two pull-up resistors should be connected, one between VCC(J3.7) and SDA pin(J1.1) and the second one between VCC(J3.7) and SCL pin(J1.4).

Please make the HW changes according to any of the mentioned options.

Note: the first HW recommendations are based on the following schematic: S32K146EVB-Q144 Evaluation Board Schematics.