Hello,
I am working on S32K146 NXP µc, and I would like to know if it is possible to manage an USB with UART ?
I know the USB has 2 wires (in fact 4, but Vcc + GND) and the voltage level are normally the same than UART.
So my first question is: is it possible to do USB with UART
My second question is: if yes, have you source code to managed the USB protocol ?
Best regards
Sebastien
Hi Razvan,
thanks for your response, this is what I thought, so you confirm.
Best regards
Sebastien
UP !!!
Hi Sebastien,
I don't think is possible because USB use D+ and D- for differential data transmission and with UART is impossible to generate differential signal because one signal is for receive and the other one is for transmit.
The good news are that on evaluation kit is included the uart <-> usb converter on the microcontroller which is used of openSDA. Check UART example.
Best regards,
Razvan