S32K146 BOOTLOADER

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K146 BOOTLOADER

Jump to solution
1,817 Views
kun_wang
Contributor II

my bootloader program jump twice time,then it can jump to app,but i do not know where the problem. and my bootloader program size is about 0xf000, in my bootload i use flash address:0x16000-0x16008 8bytes to store a flag,but when i write flag in this address, bootload cannot jump into app.please help me to solve my question, thank you advance.

0 Kudos
Reply
1 Solution
1,661 Views
kun_wang
Contributor II

thanks for your answer. the start address of the bootloader is 0,application is 0x18000,i have disabled interrupts before the jump.

yesterday i found that when i write 8 bytes the flash in 0x16000, the application can not run. I think bootloader has already jump into application,but application didn't run.when 0x16000 data is 0xFF,the application run ok. i donot know whethe the flag can stop the APP startup progress.

View solution in original post

0 Kudos
Reply
3 Replies
1,661 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

What is the start address of the bootloader and application?

Have you disabled interrupts before the jump?

Thank you.

Best regards,

Diana

0 Kudos
Reply
1,661 Views
kun_wang
Contributor II

 i found the reason :read flash make the problem, i use  ((*(__IO uint32_t*)(0x16000))) to read flash, but it can cause a

 DefaultISR:
    b       DefaultISR

0 Kudos
Reply
1,662 Views
kun_wang
Contributor II

thanks for your answer. the start address of the bootloader is 0,application is 0x18000,i have disabled interrupts before the jump.

yesterday i found that when i write 8 bytes the flash in 0x16000, the application can not run. I think bootloader has already jump into application,but application didn't run.when 0x16000 data is 0xFF,the application run ok. i donot know whethe the flag can stop the APP startup progress.

0 Kudos
Reply