S32K144UFT PDB to Trigger ADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144UFT PDB to Trigger ADC

1,777 Views
佳豪殷
Contributor I

Hi,

         when i use software to trigger ADC1 channel a ,the result in Ra is 0x0804. But, when i use PDB1 to trigger ADC1,the in Ra is changed to 0x0878.  Other  configuration  is all the same. I sample a voltage  from  2.5V reference source.

         how can i find the problem?

Labels (1)
0 Kudos
Reply
2 Replies

1,061 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

There is no reason why it would be different.

I have tested both triggers on ADC1 channel A and the result are identical.

Regards,

Daniel

0 Kudos
Reply

1,061 Views
佳豪殷
Contributor I

Thank you for you reply!

         It has been resolved .the reason  is from Self-Calibration mode.

         Before,  i do like this. Step one,  select hardware trigger mode. Step two, run Self-Calibration. Step three, use PDB to trigger  ADC1.then Ra is different.

         Now, i do like this. Step one,  select software trigger mode. Step two, run Self-Calibration. Step three, select hardware trigger mode .Step four, use PDB to trigger  ADC1.Then, Ra is identical.

        

0 Kudos
Reply