Hello, i want to recive, send data over J7 Usb connection / this is the same which is used for debugging.
I need to write a program on S32K144.
Execution of subprogrtamms should be controlled commands over Uart.
Did someone knows good example program or can give me some informations?
There are RTD, SDK and baremetal examples for LPUART that use the OpenSDA port (PTC6 / PTC7) on the EVB.
The baremetal example is included in S32DS IDE v2.2. and in the cookbook:
https://www.nxp.com/docs/en/application-note/AN5413.pdf
https://www.nxp.com/webapp/Download?colCode=AN5413SW&docLang=en
If you need RTD, use S32DS IDE v3.4.
Regards,
Daniel