S32K144EVB Send Data over CDC / someone knows? or has a example for Uart driven command execution

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144EVB Send Data over CDC / someone knows? or has a example for Uart driven command execution

372 Views
frankmuenzner7421
Contributor II

Hello, i want to recive, send data over J7 Usb connection / this is the same which is used for debugging.

I need to write a program on S32K144.

Execution of subprogrtamms should be controlled commands over Uart.

Did someone knows good example program or can give me some informations?

 

0 Kudos
Reply
1 Reply

339 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @frankmuenzner7421,

There are RTD, SDK and baremetal examples for LPUART that use the OpenSDA port (PTC6 / PTC7) on the EVB.

The baremetal example is included in S32DS IDE v2.2. and in the cookbook:

https://www.nxp.com/docs/en/application-note/AN5413.pdf

https://www.nxp.com/webapp/Download?colCode=AN5413SW&docLang=en

 

If you need RTD, use S32DS IDE v3.4.

 

Regards,

Daniel

0 Kudos
Reply