S32K144 watchdog

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K144 watchdog

487 次查看
Rohith04
Contributor II

Hi Team,

I can see a watchdog timer inside the S32K144.

How it works, as per my understanding it will automatically resets the MCU if there is any issue. Are there any hardware configuration needs to take care of?

 

If we are using external watchdog any suggestion on this?

0 项奖励
回复
1 回复

469 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Rohith04,

There are SDK and RTD WDOG examples:

SDK: wdog_interrupt_s32k144

RTD: Wdog_Ip_Example_S32K144

 

Since the WDOG is a part of the functional safety, refer to the S32K1xx Safety Manual (available in S32K1xx Secure Files).

S32K1xx SM, rev.7.1, Section 5.6.9 Watchdog timer (WDOG)

It also discusses use of External WDOG in Section 4.1 Hardware requirements on system level

 

Regards,

Daniel

0 项奖励
回复