S32K144 is stuck

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
884件の閲覧回数
kmh48301
Contributor IV

Hi

 

I inserted csec key and I Erased first sector in Pflash (0x0 address)

 

so, when i plug in debugger, it tries to mass erase. but because it has csec key, mass erase doesn't work.

 

I need to use this s32k144-evb-q100.... 

 

Please help me.

 

Thanks

Best Regards

Phillip

0 件の賞賛
返信
1 解決策
871件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Phillip,

in short - there's no way to recover.

If the flash configuration field is erased, FSEC is 0xFF and the device is secured. To unsecure the device, it's necessary to perform mass erase. But if CSE is enabled, mass erase cannot be exeucted. It would be necessary to destroy the partition using CMD_DBG_CHAL and CMD_DBG_AUTH when you need to also know MASTER_ECU_KEY. There's no way to escape this circle.

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
872件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Phillip,

in short - there's no way to recover.

If the flash configuration field is erased, FSEC is 0xFF and the device is secured. To unsecure the device, it's necessary to perform mass erase. But if CSE is enabled, mass erase cannot be exeucted. It would be necessary to destroy the partition using CMD_DBG_CHAL and CMD_DBG_AUTH when you need to also know MASTER_ECU_KEY. There's no way to escape this circle.

Regards,

Lukas

0 件の賞賛
返信