S32K144 and open draing GPIO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144 and open draing GPIO

1,587件の閲覧回数
michal_sladecek
Contributor I

Hello,

Regarding to reference manual, there should be possible to set open drain for GPIO output.

"The device does not support open drain on all the pins. Only pins that are configured for a protocol that requires open-drain(e.g;, LPI2C, LPUART single-wire) will work in open-drain mode." - Chapter 4, Signal Multiplexing and Pin Assignment

If i use GPIO on FLEXIO line it should be possible. Unfortunately, I did not find any register where is possible to set open drain option.

Can you describe this function more to me?

Thanks,

Michal

タグ(2)
2 返答(返信)

1,444件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Michal,

Unfortunately, the ports in the GPIO mode do not support Open-drain.
Only when a port is routed to a module that supports that, like LPI2C.

pastedImage_1.png

Regards,

Daniel

1,445件の閲覧回数
michal_sladecek
Contributor I

Ok, thank you for info

0 件の賞賛
返信