S32K144 Use DMA SSIZE&DSIZE is 32-byreburst

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 Use DMA SSIZE&DSIZE is 32-byreburst

Jump to solution
486 Views
lengrudie
Contributor III

Use DMA to transfer data from array to array.However, the transmission failed. The VLD, DAE, SAE, ERRCHN of the ES are set to 1. The manual says that the source address and destination address are incorrect.

My configuration is as follows:

TCD1.SADDR and DADDR both point to different arrays. The array length is 64 bytes.The SMOD and DMOD of ATTR are both 0, and the SSIZE and DSIZE are both 5 (32 byte burst).ATTR=0x0505,NBYTES_MLNO=0X40,SOFF=0X20, DOFF=0X20,CITER=1,BITER=1.

 

Thanks!

0 Kudos
Reply
1 Solution
475 Views
lengrudie
Contributor III

I've solved the problem. I found the problem. It's the address problem.

View solution in original post

0 Kudos
Reply
2 Replies
476 Views
lengrudie
Contributor III

I've solved the problem. I found the problem. It's the address problem.

0 Kudos
Reply
343 Views
Higgs_Boson
Contributor I

Hi,

 

  I have the same issue, Could you descript how to solve it?

 

 

Thanks

0 Kudos
Reply