The function FLEXCAN_EnterFreezeMode is defined in flexcan_hw_access.c file included in the SDK RTM4.0.3 flexcan example application.
The following code is included:
#if defined(ERRATA_E9595)
/* Check Low-Power Mode Acknowledge Cleared */
while (((base->MCR & CAN_MCR_LPMACK_MASK) >> CAN_MCR_LPMACK_SHIFT) == 1U) {}
... ...
#endif
Do I need to define the macro ERRATA_E9595 for S32K144 or S32K146?
Hi,
this errata is not valid for S32K1xx so it is not needed to have this macro defined.
BR, Petr