Hello,
I am trying to get the read functions to work on my ISELED development kit.
Unfortunately this does not work for me yet. I already have problems with the temperature measurement of the ISELEDs:
appState = OPERATION_ONGOING;
digLED_Read_Temp(&tempResult, strip);
while(appState == OPERATION_ONGOING);
What's wrong with this code?
Ist there a sample code for temperature Measuring?
And if it works how can i see the temperature? In the "expressions" window?
Thanks for your help!
Best regards
Oliver
Hi Oliver,
Please refer the iseled_freemaster_s32k144 example in SDK.
The actual device temperature is obtained via an integrated analog-digital converter (ADC). Then communicate temperature data with S32K.
So I think you can read the datasheet of INLC100Q16 Inova Semiconductor.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello,
thank you very much for the answer!
I got the code they provided to run. Thank you very much for that. However, I'm still not completely comfortable with the result: Here's a picture of the data I got.
How can I now read the current temperature from it?
Many thanks and best regards
Oliver