S32K144 IIC communication question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 IIC communication question

2,082 Views
asd046012
Contributor III

Hello

     I want to use the IIC fucntion of mcu s32K144,but I didn't want to use the process expert code  to generate IIC function code.

      After I configured these register,and initial the IIC register.I write the 0x04 command and one byte data to register MTDR, according to IIC communication protocal, then I should waite for transmission to end ,and check the ACK of slave device,for the ACK I check all register,and didn't have the ACK flag,so How can I judge the success of this send and start sending the next byte of data?

0 Kudos
5 Replies

1,583 Views
asd046012
Contributor III

When IIC communciation occur error for sending address and data,The NACK flag will be detected,but this flag can't be the ending flag of  sending data and address.I want to know that after send a data or address, I should check which register bit?   and how I judge that this sending action has been finished,and I can send the next data.

0 Kudos

1,583 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

There is no such bit, you can fill the transmit FIFO with commands and data and expect ACK. "Multiple transmit and receive commands can be inserted between the START condition and STOP conditon; transmit and receive commands must not be interleaved..." (50.4.2.1 RM rev.9).

If NACK is received, the master will transmit a STOP condition and will not initiate a new START condition until NACK Detect Flag has been cleared. The transfer is complete when a Stop condition has been generated.

pastedImage_1.png

pastedImage_2.png

Regards,

Daniel

0 Kudos

1,583 Views
asd046012
Contributor III

Hello  

    If I can check like this:after transfer a data,I check the bit TDF of register MSR,if the bit TDF is set as 1,I will think the transfer action has end?

   I inintail the IIC function as below sequence:

  

uint32_t tmp = 0x00000000;
IIC_DRIVER_BASE->MCR = 0x00000002;
Delay_20us();
/**disable IIC**/
IIC_DRIVER_BASE->MCR = 0x00000000;
IIC_DRIVER_BASE->MSR = 0x00000000;
/***set clock Prescaler and diable match fucntion
***set pin fucntion and NACK
***/
IIC_DRIVER_BASE->MCFGR1 = 0x00000000;
/**set baud 100K**/
IIC_DRIVER_BASE->MCCR0 = 0x0D1A1A34;
/***disable all IIC interrupt**/
IIC_DRIVER_BASE->MIER = 0x00000000;
/**disable IIC DMA Fucntion**/
IIC_DRIVER_BASE->MDER = 0x00000000;

IIC_DRIVER_BASE->MCFGR0 = 0x00000000;
IIC_DRIVER_BASE->MCFGR2 = 0x00000000;
IIC_DRIVER_BASE->MCFGR3 = 0x00000000;
IIC_DRIVER_BASE->MDMR = 0x00000000;
IIC_DRIVER_BASE->MCCR1 = 0x00000000;
IIC_DRIVER_BASE->MFCR = 0x00000000;

/**enable IIC**/
tmp = (uint32_t)IIC_DRIVER_BASE->MCR;
tmp &= (uint32_t)(~(LPI2C_MCR_MEN_MASK));
tmp |= LPI2C_MCR_MEN(0x00000001);
IIC_DRIVER_BASE->MCR = tmp;

after executing the sequence,the valeu of register MSR is alway 0x02000001,so I can solve this issue?

0 Kudos

1,583 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

The MSR[TDF] flag is set whenever the number of words in the transmit FIFO is equal or less than TXWATER.

But all transfers begin with a START condition and are terminated by a STOP stop condition.

And there is a flag MSR[SDF] that is set whenever the master generates a STOP.

UM10204 I2C-bus specification and user manual.

Example_S32K144_I2C_Master_MPL3115A2_S32DSR1_v3 

BR, Daniel

0 Kudos

1,583 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,
There is NACK Detect Flag in the Master Status register MSR[NDF] that is set whenever the master detects a NACK when transmitting an address or data.
When set, the master will transmit a STOP condition and will not initiate a new START condition until NACK Detect Flag has been cleared.

BR, Daniel

0 Kudos