S32K144 I2C Example stopped with RTOS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144 I2C Example stopped with RTOS

1,714件の閲覧回数
cheoljin
Contributor III

Hello, I am using S32K144 EVB board and S32DS3.4 to develop a program to read data through the I2C. 

But I2C example do not work after adding RTOS as below. 

cheoljin_0-1632829023856.png

IDE Version :   S32DS3.4

Example :   lpi2c_master_s32k144 + RTOS

Target : S32K144 EVB

 

The other thing is below wornning occurred when I start debugging. 

Warning 17927. Target MCU mismatch. Download performance limited. See http://www.pemicro.com/opensda/pe_tools.cfm for information on debugging external processors.
Target has been RESET and is active.
CMD>CM C:\NXP\S32DS.3.4\eclipse\plugins\com.pemicro.debug.gdbjtag.pne.expansion_5.1.0.202109011413\win32\gdi\P&E\supportFiles_ARM\NXP\S32K1xx\freescale_s32k144f512m15_pflash_dflash_eeprom.arp

Thanks. 

0 件の賞賛
返信
4 返答(返信)

1,653件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @cheoljin,

It could be a fault exception.

Please follow these instruction to find the fault instruction and the fault memory address in case of a bus fault.

https://community.nxp.com/t5/S32K-Knowledge-Base/Fault-handling-on-S32K14x/ta-p/1114447

 

Regards,

Daniel 

0 件の賞賛
返信

1,699件の閲覧回数
cheoljin
Contributor III

As I attached capture, it jump to DefaultISR. 

It looks I2C's interrupt priority issue.  

0 件の賞賛
返信

1,696件の閲覧回数
TomLightning
Contributor III

I am a bit confused due to that your attached project does not use FreeRTOS. It does not start a FreeRTOS scheduler at all. If you think it is a priority issue try to give it a logical lower priority (numerical higher). You can use functions of the interrupt manager driver from NXP for that.

0 件の賞賛
返信

1,709件の閲覧回数
TomLightning
Contributor III

Hello,

at which code section exactly does your code crash? Please, go step by step through your code in Debug Mode.

Best regards,

Tom

0 件の賞賛
返信