How to get latest version of BOOTUPDATEAPP_Pemicro?
With version BOOTUPDATEAPP_Pemicro_v111, I am getting application error. 8 times LED blinking.
Can I get the latest version of BOOTUPDATEAPP_Pemicro_v113 ?
Hello Robin,
I have contacted PE Micro support. They also given multiple troubleshooting option and finally gave-up.
According to them latest version v113 is not available for public.
Anyway I am planning to return/replace the eval board to NXP.
After going through the NXP blog, I have noticed that the issue related to Open SDA was very frequent.
But still there is no stable solution...
Have you tried to program S32K144 in S32DS?
Please refer to discussion: S32K144 D2 RED LED is ON always
Hi
OpenSDA Firmware (MSD & Debug) Firmware Apps (.zip file) can be download from https://www.pemicro.com/opensda/
But I can only find the older version ...\Pemicro_OpenSDA_Debug_MSD_Update_Apps_2020_05_12\OpenSDA_Bootloader_Update_App_v111_2013_12_11\BOOTUPDATEAPP_Pemicro_v111.SDA
For the latest BOOTUPDATEAPP_Pmicro_v113, I suggest you consult https://www.pemicro.com/support/index.cfm
Does your computer recognize the board as BOOTLOADER or S32K144EVB drive? Have you try to drop MSD-DEBUG-EVB-S32K144_Pemicro_v119.SDA to BOOTLOADER?
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks Robin.
I can go to bootloader mode(BOOTLOADR) with jumper settings.
Under boot mode, I have tried to update the open SDA(BOOTUPDATEAPP_Pemicro_v111.SDA).
After power RESET, updated with MSD-DEBUG-EVB-S32K144_Pemicro_v119.SDA to BOOTLOADER.
But when I am trying to load the application file drag and drop under S32K144EVB drive , the green LED indicator is showing application error( 8 times blink, 2 sec wait)...
I have a new s32k144 eval board RevC. It was working first day, somehow the communication error with S32DS started.
Doubting the bootloader compatibility issue...