Hello,
I have encountered problems during trying to enable the Csec feature on S32K144, and to do so, the first step I tried is to partition the flexNVM to 32K/32K and I found out that when the FCCOB1 is set to non-zero while the rest of FCCOB is set to exact same as Figure 5 in AN11983, then the operation is failed with FSTAT->ACCERR set.
For your information,
解決済! 解決策の投稿を見る。
@lukaszadrapa thank you, after checking, the order information of MCU I used is S32K144HFVLH and the 'F' indicates "CANFD FlexIO" without security. I guess the higher version MCU of the S32K144 needs to be used to enable the Csec
Hi,
this is working on my side. Which part number do you have exactly? Could you confirm it is device with CSEc?
or if you have older device:
Regards,
Lukas
@lukaszadrapa thank you, after checking, the order information of MCU I used is S32K144HFVLH and the 'F' indicates "CANFD FlexIO" without security. I guess the higher version MCU of the S32K144 needs to be used to enable the Csec