I get the demo from unified bootloader framework, but it could not work with the PLL enable, and when the project init clock, it goes to hardware error. On the other hand, if I set the PLL false, it could works. I do not know where the error is. Besides the EXTAL of my board is 16MHz, is there any wrong with the hardware designing?
解決済! 解決策の投稿を見る。
This routine uses an 8M external clock crystal oscillator by default. If you use a 16M crystal oscillator, there will be problems. You need to change the clock configuration, or replace the crystal oscillator with 8M. If you don't change the crystal oscillator, you have to change the configuration of the clock part of the BT and APP routines.
Hi Senlent,
Thanks for you response.
I have not been familiar with PLL configuration, could you please give me some suggestions that how to configure with it?
try this configuration.
Do you mean that way to modify the configuration?
yes, please have a try.