Hi,
I'm using S32 Design Studio with S32K144 (with the drivers provided by NXP), how can I use 3-wire SPI on the S32K144 in conjunction with the drivers?
I need to interface with a chip that only provides 3 pins:
* Clock
* Chip Select
* Data Input/Output
Do I need to make any HW Modifications? (e.g. something like this? Interfacing with 3-wire SPI – Total Phase)
Hi Razvan,
Thank you for replying. Based on the datasheet, the protocol should be supported, although it's called "half-duplex" or "single wire" (see screenshots below), by the way, I wish the datasheet had a section on how to use that mode (what registers to modify with what values) instead of searching all over the chapter for "half-duplex" or "single wire".
I'm trying to use the LPSPI driver provided as part of the S32K SDK, but it seems that it's designed with a full-duplex SPI connection in mind.
I tried the HW modification while calling the LPSPI_DRV_MasterTransferBlocking function but I get whatever was sent on the Rx buffers.
Hi,
Probably the right therm is LPSPI doesn't have "native support" for 3-wire because the work-flow is totally different.
Now, let's get back to your problem.
Please answer to the following questions:
1. what is the frame size in LPSPI configuration?
2. what is the size of the rx/tx in your 3-wire protocol?
3. How do you call LPSPI_DRV_MasterTransferBlocking function?
Best regards,
Razvan
1. I set it up to 8-bit
2. To read from the device: Write 8 bits of register address and then read 8 bits for the value.
3. I tried different ways:
- Sending a TxBuffer and a RxBuffer of 2 bytes each.
- Calling it once to write the address (1 byte) and then calling it again to read the address.
I checked the driver and by default it calls the following function, which means that it's the pins are configured for 2 Data Lines, am I right?
(void)LPSPI_SetPinConfigMode(base, LPSPI_SDI_IN_SDO_OUT, LPSPI_DATA_OUT_RETAINED, true);
Hi,
Please try the following set-up:
Configure the frame size to 16 bit and send with LPSPI_DRV_MasterTransferBlocking 2 bytes.
I suppose that your frame size is 8, so after 8 bits the cs toggle, so your device logic is reset. I think you should keep CS negated during all 16 bits.
Yes, the driver configures the pins for 2 data lines.
Best regards,
Razvan