S32K142 hard fault error when clocking core with pll clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K142 hard fault error when clocking core with pll clock

跳至解决方案
5,114 次查看
TomLightning
Contributor III

Hi,

I want to clock the core (CORE_CLK, SYS_CLK, BUS_CLK, FLASH_CLK) by using the PLL clock as source. My prefered clock frequencies are the following:

  • CORE_CLK - 80MHz
  • SYS_CLK - 80MHz
  • BUS_CLK - 40MHz
  • FLASH_CLK - 26.67MHz

Please see below my clock config struct:

clock_manager_user_config_t clockMan1_InitConfig0 = {
    /*! @brief Configuration of SIRC */
    .scgConfig =
    {
        .sircConfig =
        {
            .initialize       = true,                                          /*!< Initialize */
            /* SIRCCSR */
            .enableInStop     = false,                                         /*!< SIRCSTEN  */
            .enableInLowPower = true,                                          /*!< SIRCLPEN  */
            .locked           = false,                                         /*!< LK        */
            /* SIRCCFG */
            .range            = SCG_SIRC_RANGE_HIGH,                           /*!< RANGE - High range (8 MHz) */
            /* SIRCDIV */
            .div1             = SCG_ASYNC_CLOCK_DIV_BY_1,                      /*!< SIRCDIV1  */
            .div2             = SCG_ASYNC_CLOCK_DIV_BY_1,                      /*!< SIRCDIV2  */
        },
        .fircConfig =
        {
            .initialize       = true,                                          /*!< Initialize */
            /* FIRCCSR */
            .regulator        = true,                                          /*!< FIRCREGOFF */
            .locked           = false,                                         /*!< LK         */
            /* FIRCCFG */
            .range            = SCG_FIRC_RANGE_48M,                            /*!< RANGE      */
            /* FIRCDIV */
            .div1             = SCG_ASYNC_CLOCK_DIV_BY_1,                      /*!< FIRCDIV1   */
            .div2             = SCG_ASYNC_CLOCK_DIV_BY_1,                      /*!< FIRCDIV2   */
        },
        .rtcConfig =
        {
            .initialize       = true,                                          /*!< Initialize  */
            .rtcClkInFreq     = 0U,                                            /*!< RTC_CLKIN   */
        },
        .soscConfig =
        {
            .initialize       = true,                                          /*!< Initialize */
            .freq             = 20000000U,                                     /*!< Frequency  */
            /* SOSCCSR */
            .monitorMode      = SCG_SOSC_MONITOR_DISABLE,                      /*!< SOSCCM      */
            .locked           = false,                                         /*!< LK          */
            /* SOSCCFG */
            .extRef           = SCG_SOSC_REF_OSC,                              /*!< EREFS       */
            .gain             = SCG_SOSC_GAIN_LOW,                             /*!< HGO         */
            .range            = SCG_SOSC_RANGE_HIGH,                           /*!< RANGE       */
            /* SOSCDIV */
            .div1             = SCG_ASYNC_CLOCK_DIV_BY_1,                      /*!< SOSCDIV1    */
            .div2             = SCG_ASYNC_CLOCK_DIV_BY_1,                      /*!< SOSCDIV2    */
        },
        .spllConfig =
        {
            .initialize       = true,                                          /*!< Initialize */
            /* SPLLCSR */
            .monitorMode      = SCG_SPLL_MONITOR_DISABLE,                      /*!< SPLLCM     */
            .locked           = false,                                         /*!< LK         */
            /* SPLLCFG */
            .prediv           = (uint8_t)SCG_SPLL_CLOCK_PREDIV_BY_2,           /*!< PREDIV     */
            .mult             = (uint8_t)SCG_SPLL_CLOCK_MULTIPLY_BY_32,        /*!< MULT       */
            .src=0U,                                            /*!< SOURCE     */
            /* SPLLDIV */
            .div1             = SCG_ASYNC_CLOCK_DIV_BY_2,                      /*!< SPLLDIV1 @ 80MHz      */
            .div2             = SCG_ASYNC_CLOCK_DIV_BY_4,                      /*!< SPLLDIV2 @ 40MHz      */
        },
        .clockOutConfig =
        {
            .initialize       = true,                                          /*!< Initialize    */
            .source           = SCG_CLOCKOUT_SRC_SIRC,                         /*!< SCG CLKOUTSEL     */
        },
        .clockModeConfig =
        {
            .initialize       = true,                                          /*!< Initialize */
            .rccrConfig =              /*!< RCCR - Run Clock Control Register          */
            {
                .src=SCG_SYSTEM_CLOCK_SRC_SYS_PLL,                  /*!< SCS        SPLL  @ 160MHz   */ 
                .divCore      = SCG_SYSTEM_CLOCK_DIV_BY_2,                     /*!< DIVCORE    Core  @ 80MHz    */
                .divBus       = SCG_SYSTEM_CLOCK_DIV_BY_2,                     /*!< DIVBUS     Bus   @ 40Mhz    */
                .divSlow      = SCG_SYSTEM_CLOCK_DIV_BY_4,                     /*!< DIVSLOW    Flash @ 26.67MHz */
            },
            .vccrConfig =              /*!< VCCR - VLPR Clock Control Register         */
            {
                .src=SCG_SYSTEM_CLOCK_SRC_SIRC,                     /*!< SCS        */
                .divCore      = SCG_SYSTEM_CLOCK_DIV_BY_2,                     /*!< DIVCORE    */
                .divBus       = SCG_SYSTEM_CLOCK_DIV_BY_1,                     /*!< DIVBUS     */
                .divSlow      = SCG_SYSTEM_CLOCK_DIV_BY_4,                     /*!< DIVSLOW    */
            },
            .hccrConfig =              /*!< HCCR - HSRUN Clock Control Register        */
            {
                .src=SCG_SYSTEM_CLOCK_SRC_SYS_PLL,                  /*!< SCS        */
                .divCore      = SCG_SYSTEM_CLOCK_DIV_BY_1,                     /*!< DIVCORE    */
                .divBus       = SCG_SYSTEM_CLOCK_DIV_BY_2,                     /*!< DIVBUS     */
                .divSlow      = SCG_SYSTEM_CLOCK_DIV_BY_4,                     /*!< DIVSLOW    */
            },
        },
    },
    .pccConfig =
    {
        .peripheralClocks = peripheralClockConfig0,                            /*!< Peripheral clock control configurations  */
        .count = NUM_OF_PERIPHERAL_CLOCKS_0,                                   /*!< Number of the peripheral clock control configurations  */
    },
    .simConfig =
    {
        .clockOutConfig =              /*!< Clock Out configuration.           */
        {
            .initialize       = true,                                          /*!< Initialize    */
            .enable           = false,                                         /*!< CLKOUTEN      */
            .source           = SIM_CLKOUT_SEL_SYSTEM_SCG_CLKOUT,              /*!< CLKOUTSEL     */
            .divider          = SIM_CLKOUT_DIV_BY_1,                           /*!< CLKOUTDIV     */
        },
        .lpoClockConfig =              /*!< Low Power Clock configuration.     */
        {
            .initialize       = true,                                          /*!< Initialize    */
            .enableLpo1k      = true,                                          /*!< LPO1KCLKEN    */
            .enableLpo32k     = true,                                          /*!< LPO32KCLKEN   */
            .sourceLpoClk     = SIM_LPO_CLK_SEL_LPO_128K,                      /*!< LPOCLKSEL     */
            .sourceRtcClk     = SIM_RTCCLK_SEL_SOSCDIV1_CLK,                   /*!< RTCCLKSEL     */
        },
        .platGateConfig =              /*!< Platform Gate Clock configuration. */
        {
            .initialize       = true,                                          /*!< Initialize    */
            .enableMscm       = true,                                          /*!< CGCMSCM       */
            .enableMpu        = true,                                          /*!< CGCMPU        */
            .enableDma        = true,                                          /*!< CGCDMA        */
            .enableErm        = true,                                          /*!< CGCERM        */
            .enableEim        = true,                                          /*!< CGCEIM        */
        },

        .qspiRefClkGating =            /*!< Quad Spi Internal Reference Clock Gating. */
        {
            .enableQspiRefClk  = false,                                        /*!< Qspi reference clock gating    */
        },
        .tclkConfig =                  /*!< TCLK CLOCK configuration. */
        {
            .initialize       = true,                                          /*!< Initialize    */
            .tclkFreq[0]      = 0U,                                            /*!< TCLK0         */
            .tclkFreq[1]      = 0U,                                            /*!< TCLK1         */
            .tclkFreq[2]      = 0U,                                            /*!< TCLK2         */
        },
        .traceClockConfig =            /*!< Debug trace Clock Configuration. */
        {
            .initialize       = true,                                          /*!< Initialize    */
            .divEnable        = true,                                          /*!< TRACEDIVEN    */
            .source           = CLOCK_TRACE_SRC_CORE_CLK,                      /*!< TRACECLK_SEL  */
            .divider          = 0U,                                            /*!< TRACEDIV      */
            .divFraction      = false,                                         /*!< TRACEFRAC     */
        },
    },
    .pmcConfig =
    {
        .lpoClockConfig =              /*!< Low Power Clock configuration.     */
        {
            .initialize       = true,                                          /*!< Initialize             */
            .enable           = true,                                          /*!< Enable/disable LPO     */
            .trimValue        = 0,                                             /*!< Trimming value for LPO */
        },
    },
};

I changing the clock settings by calling the following function at the beginning of main:

CLOCK_DRV_Init(*g_clockManConfigsArr);

When I try to access registers of peripherals I get a hard fault error. Do you have an idea what can cause that problem? When I clock the system by using FIRC as source, everything works well.

Best regards

Tom

0 项奖励
回复
1 解答
4,955 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@TomLightning

I tried to configure according to the configuration file you sent me. I found that the clock configuration tool reported an error. You can change this place and test it again.

Senlent_0-1636528186333.png

Senlent_1-1636528220856.png

 

            .hccrConfig =              /*!< HCCR - HSRUN Clock Control Register        */
            {
                .src=SCG_SYSTEM_CLOCK_SRC_SYS_PLL,                  /*!< SCS        */
                .divCore      = SCG_SYSTEM_CLOCK_DIV_BY_2,                     /*!< DIVCORE    */
                .divBus       = SCG_SYSTEM_CLOCK_DIV_BY_2,                     /*!< DIVBUS     */
                .divSlow      = SCG_SYSTEM_CLOCK_DIV_BY_4,                     /*!< DIVSLOW    */
            },

 

BR!

     Jim,

在原帖中查看解决方案

12 回复数
5,098 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@TomLighting

         I did the test as you said. like below, it works fine on my side. Hardware based on S32K142EVB,the Crystal oscillator is 8M, however I found that you set crystal oscillator Frequency at 20M, so please check you Crystal oscillator .

S32K142EVB,crystal oscillator 8MHz.

Senlent_0-1635471441361.png

 Please check red line highlight,

Senlent_1-1635471528310.png

The attachments  was create by me, for reference only.

 

BR!

     Jim,

0 项奖励
回复
5,091 次查看
TomLightning
Contributor III

Hi Jim,

the S32K142 is placed on a PCB designed on my own. The external oscillator has a resonance frequency at 20MHz. But I have an idea what could cause the trouble. The Datasheet says, that the reference clock of the PLL must lie between 8 and 16MHz what would implicate that I have to set the reference clock divider to two (0b001). Could that be the problem?

Best Regards

Tom

5,080 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@TomLightning

         I think this may be the reason. 16MHz can work normally, I have seen related applications but I don't have a 20MHz crystal oscillator, so I can't test it.

BR!

     Jim,

0 项奖励
回复
5,050 次查看
TomLightning
Contributor III

Hi,

the predivider was already set to two. So this option is not causing the problem. Any other suggestions?

Best Regards

Tom

0 项奖励
回复
5,012 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@TomLightning

1.Refers to: AN5408

        The SOSC can source from either a signal driven into the EXTAL pin or a crystal oscillator connected to the XTAL and EXTAL pins (henceforth referred as simply “XTAL).EXTAL can support up to 50 MHz, while there are two ranges that are allowed for the XTAL depending on configuration: 4-8 MHz or 8-40 MHz;

Senlent_0-1636441038018.png

So, we can pretty sure that 20MHz XTAL is supported by S32K142.

---------------------------------------------------------------------------------------------------------------------------

2.Then we discuss about reason that cause the error. 

That was your configuration.

Senlent_2-1636441853694.png

Clock configurate Tool show error.

Senlent_1-1636441663389.png

Limits.

SPLL_VCO_CLK (min) 180
SPLL_VCO_CLK (max) 320

 

and about Flash clock.

Senlent_3-1636442343844.png

If you want set Flash clock = 26.667MHz, then  .divSlow = SCG_SYSTEM_CLOCK_DIV_BY_3,

-------------------------------------------------------------------------------------------------------------------------------

Try this configuration.

Senlent_4-1636442616201.png

 

BR!

     Jim,

---------------------------------------------------------------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
---------------------------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
5,002 次查看
TomLightning
Contributor III

Hi Jim,

i agree with the flash-clock option. But when I type the following configuration into the clock calculator AN5408SW it says that everything should work fine:

.rccrConfig =              /*!< RCCR - Run Clock Control Register          */
            {
                .src=SCG_SYSTEM_CLOCK_SRC_SYS_PLL,                  /*!< SCS        SPLL  @ 160MHz   */ 
                .divCore      = SCG_SYSTEM_CLOCK_DIV_BY_2,                     /*!< DIVCORE    Core  @ 80MHz    */
                .divBus       = SCG_SYSTEM_CLOCK_DIV_BY_2,                     /*!< DIVBUS     Bus   @ 40Mhz    */
                .divSlow      = SCG_SYSTEM_CLOCK_DIV_BY_4,                     /*!< DIVSLOW    Flash @ 26.67MHz */
            },

 Best regards

Tom

0 项奖励
回复
4,992 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@TomLightning

Sorry i read wrong

My colleague suggested to check Hardfault's specific reasons first.

Can you use an oscilloscope to detect the waveform? Is the clock waveform correct?

If the predivider is set larger, such as 4, will it work?

Our laboratory does not have a 20MHz crystal oscillator. Otherwise, I can help you reproduce the problem quickly. I can only guess the possible cause.

Can you send me your clock configuration file, let me double check.

BR!

     Jim,

 

 

0 项奖励
回复
4,987 次查看
TomLightning
Contributor III

Maybe the following information may also help you:

When I do operations in a while-loop which are not accessing peripheral registers everything works fine.

 

 

CLOCK_DRV_Init(*g_clockManConfigsArr);

int x = 0;

while(1)
{
   x++;
}

 

 

I will check the waveform of the oscillator and will test some other configurations.

Best regards

Tom

Edit:

Here are the shots from the oscilloscope.

Extal_PinExtal_PinXtal_PinXtal_Pin

0 项奖励
回复
4,956 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@TomLightning

I tried to configure according to the configuration file you sent me. I found that the clock configuration tool reported an error. You can change this place and test it again.

Senlent_0-1636528186333.png

Senlent_1-1636528220856.png

 

            .hccrConfig =              /*!< HCCR - HSRUN Clock Control Register        */
            {
                .src=SCG_SYSTEM_CLOCK_SRC_SYS_PLL,                  /*!< SCS        */
                .divCore      = SCG_SYSTEM_CLOCK_DIV_BY_2,                     /*!< DIVCORE    */
                .divBus       = SCG_SYSTEM_CLOCK_DIV_BY_2,                     /*!< DIVBUS     */
                .divSlow      = SCG_SYSTEM_CLOCK_DIV_BY_4,                     /*!< DIVSLOW    */
            },

 

BR!

     Jim,

4,945 次查看
TomLightning
Contributor III

Hi Jim,

finally it is working! But I don't understand why the high speed run settings do affect the microcontroller operation in normal mode. Anyways, it works!

Is it okay, that the sine wave looks so distorted at the XTAL_Pin. Or should I try to operate the SOSC in the high gain mode? What is the advantage of operating the SOSC in the high gain mode? I guess it is more stable but more power consuming as well.

Maybe you can send me oscilloscope shots from the evaluation board as reference?

Best regards
Tom

0 项奖励
回复
4,924 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@TomLightning

        Finally solved the problem!

        Sorry for the late reply, cause the time zone.

        As I said above, I only have an 8MHz crystal oscillator. Do you need me to record the waveform and send it to you? 

BR!

     Jim,

0 项奖励
回复
4,900 次查看
TomLightning
Contributor III

This would be nice. Can you also add the information if the resonator is operated with low or high gain please?

Best regards

Tom

0 项奖励
回复