S32K142 flexcan dominant detection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K142 flexcan dominant detection

ソリューションへジャンプ
643件の閲覧回数
FanJialin
Contributor II

Hello,

I used flexcan's RxFIFO for CAN development.

How can I detect dominant time-out through flexcan or other methods.

What interrupts or interfaces does flexcan have?

Dominant time-out refers to the detection of the SOF segment of the CAN frame as shown in the figure

20240408-104648.jpg

0 件の賞賛
返信
1 解決策
579件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

1) No, just IDLE, TX and RX bits of ESR1 shows that something is on the bus.
2) there is no indication for a message that is not matched in neither MB nor RXFIFO, frame is lost.

BR, Petr

元の投稿で解決策を見る

3 返答(返信)
616件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

why would dominant time-out refer to the detection of the SOF segment? SOF is single dominant bit and is normally detected by module. Long time dominant condition will be detected via stuff or form errors and error interrupt will be called if enabled. Module tolerates 5 consecutive dominant bits then stuff bit (opposite level) must be detected.
Dominant time out feature is obviously implemented on CAN transceiver to disable transmitter when TXD line is held low for extended/defined time, so a node will not disturb bus anymore.

BR, Petr

587件の閲覧回数
FanJialin
Contributor II

Sorry, there was an error in my description. Let me rephrase the problem.
1.Can flexcan notify me through interrupts or other means when it changes from an recessive state to an dominant state on the CAN bus.
2.Can flexcan notify me through interrupts or other means when receiving frames outside of the filter.

0 件の賞賛
返信
580件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

1) No, just IDLE, TX and RX bits of ESR1 shows that something is on the bus.
2) there is no indication for a message that is not matched in neither MB nor RXFIFO, frame is lost.

BR, Petr