S32K

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K

243件の閲覧回数
zq1
Contributor III

i am building a project with S32K312 ,but the flexcan can not run ,it can not enter interupt recieive  data or send data,so i want to a example ,maybe the hardware is wrong or software ,thank you very much.

0 件の賞賛
1 返信

226件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please refer to the Example S32K344 FlexCAN_Ip TX/RX/EnhanceRXFIFO test S32DS3.4 RTD200. Although it is not based on S32K312, the configuration of FlexCAN Driver in S32 Configuration Tool is similar. 


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛