Dears,
Actually, I need S32KNHT1MPBST for my project, but now I only have S32KEHT1MPBST on hand, so here I want to know if they have hardware level diff between of them? or the difference is only about the IPs in them, and I can replace S32KNHT1MPBST with S32KEHT1MPBST completley?
thanks a lot~
解決済! 解決策の投稿を見る。
Hi, could you please double check mentioned part numbers? I don't think these are existing devices. Are they supposed to be MCUs or some boards / other equipment? Please clarify
Hi, Sorry, I forgot the "344", it should be S32K344NHT1MPBST and S32K344EHT1MPBST.
The only difference is missing Ethernet, in other aspect both derivatives are equal.
That means both can be used to replace each other pin 2 pin on hardware level if Ethernet was not used, that is right?
Yes, it is.
got it ,thanks a lot~