S32K I2C open drain FET resistance

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K I2C open drain FET resistance

1,368 次查看
Alex_Raisle
Contributor I

Hello everybody,

i use I2C at the S32K144 with external Pull Up Resistor.

Is there a specification about the Rds_on of the internal FET which pulls the line down to GND?

Alex_Raisle_0-1675762036368.png

 

Best regards, Alex

0 项奖励
回复
4 回复数

1,339 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Rds_on is not typically given on the MCU's datasheet. The specification given is the current it can handle.

UM10204 gives a brief explanation on how to calculate the minimum and the maximum Pull-up resistor [Page 50, UM10204, Rev 7.0, 10/2021] with typically given electrical specifications.

Please, let us know if this information was helpful or not.

0 项奖励
回复

1,323 次查看
Alex_Raisle_
Contributor I

Hello,

in the UM10204 chapter 4.2.3 is written "NXP devices have a higher power set of electircal characteristics than SMBus 1.0. The main difference is the current sink capability with Vol = 0.4V."

Due to the Reference Manual Rev. 10 chapter 50.2 "The LPI2C module also compiles [..] (SMBus) Specification, version 2.

So due to this I assume that Vol = 0.4V at this µC if I limit the current to 3mA?

Best regards, Alexander

0 项奖励
回复

1,318 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For the case of S32K1xx, datasheet shows V_OL(max) as 0.8V and I_OL as 5mA (Whitin IolGPIO-HD_DSE_0 @ 5V). With this, you will have the minimum value for Rp, anything above that (and below the maximum Rp calculated with Eq 1) should be fine.

These should be the values that UM10204 refers to.

Please, let us know.

0 项奖励
回复

1,330 次查看
Alex_Raisle_
Contributor I

Hello Daniel,

thank you for the information.

In the datasheet I only find the information that at 0.8V the min. current is 5mA.

How high is the voltage for example at 3mA?

Is there a graph or a data table available?

Best regards, Alexander

0 项奖励
回复