S32K Data retention (in data-flash)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K Data retention (in data-flash)

1,957 Views
yvesbriant
NXP Employee
NXP Employee

The Data-sheets v1 specify a min and typ data retention for the data-flash. The typical number corresponds to an average temperature of 25°C and to nominal supply voltages. How is the minimum number defined (average temperature, supply levels)?

We used to have the EB618 (attached) to explain the way data retention is specified for various technology, but it is now outdated. It would be great to have a table similar to table 1, including the TFS90 technology:

Tags (1)
0 Kudos
Reply
3 Replies

1,496 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Yves,

minimal data retention is always valid across whole temperature range and whole supply voltage range. Conditions for typical data retention are explicitly mentioned in datasheet (25°C...).

Regards,

Lukas

0 Kudos
Reply

1,496 Views
yvesbriant
NXP Employee
NXP Employee

Hello Lukas,

That's what i told to my customer, but they need more details. For the S12Z devices, we explicitly specify the average temperature we considered for the min specification for the data retention (see below), here 85°C. I would be interested to know what average temperature we considered for the S32K.

Capture.PNG

1 TJavg does not exceed 85C in a typical temperature profile over the lifetime of a consumer, industrial or automotive application.

2 Typical data retention values are based on intrinsic capability of the technology measured at high temperature and de-rated to 25C using the Arrhenius equation. For additional information on how Freescale defines Typical Data Retention, please refer to Engineering Bulletin EB618

Thanks !

0 Kudos
Reply

1,497 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

I sent you an email...

Lukas

0 Kudos
Reply