Hi everyone,
What I saw a post just now is the same as my subject. when I install the offline installation package, I also found I can't install freertos, reporting one or more required tiems could not be found. image as follows:
it show that I had installed the software., nstallation details as follows:
but I can't create new freertos project from k3 example, images as follows:
how do I install successfully?
Solved! Go to Solution.
Hi @Hanoch
The FreeRTOS version 2.0.3 was developed for S32DS v3.4 using S32K3 Real-Time Drivers AUTOSAR 4.4 Version 2.0.3. According to the provided information, you are using S32DS v3.5 and RTD v3.0.0; the FreeRTOS version compatible with this SW is the 3.1.0 (SW32K3_FreeRTOS_10.5.1_3.1.0_D2304).
B.R.
VaneB
Hi @Hanoch
The FreeRTOS version 2.0.3 was developed for S32DS v3.4 using S32K3 Real-Time Drivers AUTOSAR 4.4 Version 2.0.3. According to the provided information, you are using S32DS v3.5 and RTD v3.0.0; the FreeRTOS version compatible with this SW is the 3.1.0 (SW32K3_FreeRTOS_10.5.1_3.1.0_D2304).
B.R.
VaneB
Thanks, it's done!