S32DS can't build freertos for S32K312

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS can't build freertos for S32K312

Jump to solution
303 Views
Ean
Contributor II

hi everyone

1.jpg2.jpg3.jpg4.jpg

When using 'SW32K3_FreeRTOS_10_5_1_UOS_3_1_0_DS_updatesite_D2304', generate routine for S32K312, compile fails.and where to download template software for S32K312EVK

 

 

 

0 Kudos
Reply
1 Solution
258 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Select the "S32 Configuration Tool" menu then click on the desired configuration tool (Pins, Cocks, Peripherals etc...).
Clicking on any one of those will generate all the components. Make the desired changes(if any) then click on the "S32 Configuration Tool->Update Code" button.

Do you still encounter errors when you build after clicking Update Code?
I refer to HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5 to install S32K3, and then install SW32K3_FreeRTOS_10_5_1_UOS_3_1_0_DS_updatesite_D2304.zip. No errors will be encountered when building.

Sorry, I haven't seen the S32K312 examples since the version after S32K3 RTD 2.0.3. As you know, S32K3 has many derivatives, so to reduce effort, in the most recent RTD releases we only provide examples for K344, K358, and K396.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
259 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Select the "S32 Configuration Tool" menu then click on the desired configuration tool (Pins, Cocks, Peripherals etc...).
Clicking on any one of those will generate all the components. Make the desired changes(if any) then click on the "S32 Configuration Tool->Update Code" button.

Do you still encounter errors when you build after clicking Update Code?
I refer to HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5 to install S32K3, and then install SW32K3_FreeRTOS_10_5_1_UOS_3_1_0_DS_updatesite_D2304.zip. No errors will be encountered when building.

Sorry, I haven't seen the S32K312 examples since the version after S32K3 RTD 2.0.3. As you know, S32K3 has many derivatives, so to reduce effort, in the most recent RTD releases we only provide examples for K344, K358, and K396.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply