S32DS about S32K146_64 SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS about S32K146_64 SDK

1,421 Views
oceansea
Contributor III

hello

i want to use the S32K146_64MCU  ,and then i use the S32DS compile the prj ,it show below:

pastedImage_1.png

ERROR: S32K146_64 processor is not supported by selected SDK SDK_S32K14x_09 located in: E:\S32DS_forARM\eclipse\ProcessorExpert/../../S32DS/S32SDK_S32K14x_EAR_0.8.6

first i think is the sdk is old ,so i update my sdk ,after update it show this

 pastedImage_2.png

my sdk is ok ,but it remain error.how to solve this

thanks .

Labels (1)
0 Kudos
9 Replies

1,215 Views
oceansea
Contributor III

Hi,

thanks reply .

this is my step to install de update

 pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

pastedImage_4.png

0 Kudos

1,215 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

Not it makes sense. Design studio provide multiple updates. The one which you have installed is just to add support for S32K146 debugging. You must install the update which adds support for S23K146 SDK software. You can check all updates available and for sure it will work fine.

Best regards,

Razvan

0 Kudos

1,215 Views
oceansea
Contributor III

Hi,

now i install all the update 

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

but it still show this 

pastedImage_5.png

pastedImage_6.png

it ask me install the KSDK 1.1,but after N time update, i still only have SDK0.8.6,  where can install KSDK 1.1?

pastedImage_1.png

0 Kudos

1,215 Views
razva_tilimpea
NXP Employee
NXP Employee

HI,

Please try the following steps:

1. Create a new work space (File -> Switch workspace -> other)

2. start new project based on SDK projects: File -> New ->S32DS Project from example

3.  Import hello world projectpastedImage_1.png

Best regards,

Razvan

0 Kudos

1,215 Views
oceansea
Contributor III

hi,

thanks reply ,i do follow your idea,is perfect

pastedImage_1.png

do this   use S32K1XX RTM SDK 3.00,then select   LQFP64    packaging ,is ok ,not any error, perfect

but i have some question :

1、SDK  have   EAR    BETA    RTM  three different  version  ,what different  about then ?

2、i creat a app prj  not use example 

pastedImage_1.png

pastedImage_2.png

pastedImage_1.png

why i can't  select  S32K1XX RTM SDK 3.00?it only have SDK 0.8.6

when i use example it can select S32K1XX RTM SDK 3.00,it indicate i really installed the S32K1XX RTM SDK 3.00

thanks.

0 Kudos

1,215 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

EAR release is early access release, in general this is the first release for a specific release

BETA release includes some fixes, but is not ready to be used in production

RTM release is fully tested and ready to be release in market and integrated in production.

For your second question I don't have an answer because I can't reproduce this on my side.

Razvan

0 Kudos

1,215 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

Your Processor Expert component is redirected to EAR 0.8.6 which probably doesn't support this CPU. I suppose that you are 

Try to create a new workspace and to import a project based on last SDK version. 

Razvan

0 Kudos

1,215 Views
oceansea
Contributor III

hi ,

thanks your reply, 

i try to follow your opinion ,but  i only hava one version SDK,and when i try install other version,it show this 

pastedImage_1.png

0 Kudos

1,215 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

Please provide me the steps to reproduce this on my side.

Razvan

0 Kudos