We are developing S32K344 MCU.
The IDE is using S32 Design Studio for S32 Platform v.3.4.
And for debugging, I am using Pemicro multilink universal.
When developing our existing project (using S32K144) (using S32DS 2.2), the “Flash” menu was displayed on the menu and icon, so we used it well.
The Flash menu is not found in S32DS v3.4.
Of course, I checked enable for the 'create flash image' option.
And i use pemicro support 5.1.4
Where can I find the Flash menu?
Or how can I add a Flash menu?
Solved! Go to Solution.
sorry,this feature is no longer supported in S32 Design Studio for S32 Platform.
okay. It's unfortunate, but I get it.
Thanks for the information.