S32DS / S32K144: holding low the UART tx pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32DS / S32K144: holding low the UART tx pin

856 次查看
Joao_Roscoe
Contributor III

I'm using UART to interface with a chip which implements a "safe mode" UART configuration in which the chip runs it's UART port with a standard, known parameters set - this allow recovering from configuration errors.

To trigger such "safe mode" I need to hold UART Tx at low, for a predefined, long time. What would be the best way to accomplish that? Changing the port configuration to GPIO, and than back to UART?

Best regards,

Joao

标记 (2)
0 项奖励
回复
1 回复

778 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

one option is to use break character which can be up to 15 bit times long. See the LPUART description for more details.

If it is not enough, then you can reconfigure the pin to GPIO.

Regards,

Lukas

0 项奖励
回复