S32DS / S32K144: holding low the UART tx pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS / S32K144: holding low the UART tx pin

854 Views
Joao_Roscoe
Contributor III

I'm using UART to interface with a chip which implements a "safe mode" UART configuration in which the chip runs it's UART port with a standard, known parameters set - this allow recovering from configuration errors.

To trigger such "safe mode" I need to hold UART Tx at low, for a predefined, long time. What would be the best way to accomplish that? Changing the port configuration to GPIO, and than back to UART?

Best regards,

Joao

Tags (2)
0 Kudos
Reply
1 Reply

776 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

one option is to use break character which can be up to 15 bit times long. See the LPUART description for more details.

If it is not enough, then you can reconfigure the pin to GPIO.

Regards,

Lukas

0 Kudos
Reply