Hi guys,
i just finished the Getting Started Section for the S32K344 .
I installed "S32 Design Studio IDE", SDK and also the Real-Time Driver.
Using " ping 192.168.225.100 -t" works fine.
Next I wanted to follow the Getting Started with S32K3 using S32DS at the hello world project Training Presentation.
Which worked fine until the debugging process. Where it cant detect my hardware.
I tried to use Ethernet as an Interface and also the J74 Type C Connector.
Are there any Drivers I have to install? My Device Manager doesnt update if I plug the USB-C in.
What are the steps so my S32 Studio can detect my S32K344 Device?
EDIT1: To be clear I don't have a PEmicro JTAG connector connected. Is there no Onboard debugging connection?
解決済! 解決策の投稿を見る。
Hello @Ojav,
The S32K344 MCU can be reprogrammed via the J40 JTAG/SWD connector only.
There is no on-board programmer/debugger.
Regards,
Daniel
Hello @Ojav,
The S32K344 MCU can be reprogrammed via the J40 JTAG/SWD connector only.
There is no on-board programmer/debugger.
Regards,
Daniel