S32 Design Studio for S32 Platform 3.5使用问题

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio for S32 Platform 3.5使用问题

764件の閲覧回数
chuanlin
Contributor III

S32K3444   +  S32 Design Studio for S32 Platform 3.5  Can I use the J-Link download method? How can I set the Debug page?

0 件の賞賛
3 返答(返信)

754件の閲覧回数
chuanlin
Contributor III

chuanlin_0-1671594761597.png

chuanlin_1-1671594797763.png

Hello, the configuration here is like this. Then the program can be downloaded through Debug, but the Resume cannot run。

Note:Break at address "0x20020000" with no debug information available, or outside of program code.

 

0 件の賞賛

744件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@chuanlin

Have you tried the demo which provided under the S32 DS?

if there is no problem with the demo provided by S32 DS, then maybe a problem with your own project.

I find some similar problems for your reference to solve.

https://blog.csdn.net/eastgeneral/article/details/84913318?spm=1001.2101.3001.6661.1&utm_medium=dist... 

0 件の賞賛

756件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@chuanlin

This should be the same as the V3.4 version, both can use J-LINK

Senlent_0-1671594512501.png

 

0 件の賞賛