Hi Nxp Team,
I have gone through the user manual of RAPPID tool and fallowed the below steps
1. Drag and drop the RBF file o the Evaluvation board
2.reset the EVAL board(connected the S32K144 Eval board with USB)
3. open the Rappid tool
4.load the rbl file (given in the example project of S32K_bootloader ,edited the path in the rbl file)
5. tool updated the all the configuration details and click on the "start the bootloader"
but it is not programmed , it is showing error "loss communication with CCP MCU, please cycle power and try again" and "operation has timed out".
I have tried with reset the controller and tried , but still getting same error.
for the application download also, manually i have set the configuration details and and disable the "BAM status" , tried to flash the Timer_test.hex file ,still it is showing same error.
find the attached errors images and please let me know the solution.
Regards,
Ambarish
Hello Stanish,
Thank you for your immediate response.
I have tried with S19 file also , still getting same error.
do I need to changes any settings in eval board(jumper connection change)?
I fallowed the steps explained in the forum by Jiri.Kral.
link is here :
https://community.nxp.com/thread/464653.
even for example code , getting the same error.
for the application flashing :
we can manually set the port configuration , disable the BAM , and tick the "erase and program" and start the bootloader.
is this correct
Thank you in advance for your help.
Regards,
Ambarish
I am even facing the same issue.
If you have resolved it could you please guide me.
I have uploaded the RBF file provided in MATLAB toolbox for UART0 CAN0.(with S32k144)
Baud Rate :115200.
But I always get Loss of Communication CPP Error.
Regards
Nisha Lemos