RappID Bootloader S32K144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RappID Bootloader S32K144

4,908 Views
koehlerl
Contributor IV

Hello,

witch UART use the RappID Bootloader in the S32K144 ?

Tags (1)
9 Replies

2,568 Views
koehlerl
Contributor IV

I need a rbf file for the S32k144 cut2 0N47T where UART0 is used instead of UART2.

Where can I get such a rbf file or is it possible to get the source code to make my one rbf file?

0 Kudos

2,574 Views
dumitru-daniel_
NXP Employee
NXP Employee

Hi koehlerl‌,

Based on my experience with S32K144 and i can confirm the RAppID_BL works with UART1 interface. I'm using the OpenSDA microUSB connector from S32K144 EVB to program the elf into flash/ram

For that you will need to flash the RBF file first (using S32DS). Have you done that ?

Best regards,
Daniel

0 Kudos

2,574 Views
koehlerl
Contributor IV

Hi Daniel,

I use the S32K144 EVB. I have flashed the rbf file first. But I can’t connect with the RappID BL tool.

The trace window of RappID BL Tool is empty an then after timeout the Error message comes:

There are different kinds of the rbf file for the s32K144 CPU?

BR Lutz

Von: dumitru-daniel.popa

Gesendet: Donnerstag, 31. August 2017 11:07

An: Köhler, Lutz <lutz.koehler@acd-antriebstechnik.de>

Betreff: Re: - Re: RappID Bootloader S32K144

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: RappID Bootloader S32K144

reply from dumitru-daniel.popa<https://community.nxp.com/people/dumitru-daniel.popa?et=watches.email.thread> in S32K - View the full discussion<https://community.nxp.com/message/938696?commentID=938696&et=watches.email.thread#comment-938696>

0 Kudos

2,574 Views
dumitru-daniel_
NXP Employee
NXP Employee

Hi Lutz, 

There are different versions of RAppID_BL.exe and different versions of RBF files.

I'm using bootloader version 1.6.5.1

pastedImage_2.png

And the RBL attached and is working fine via the micro-usb

Here is a snapshot programming the S32K144EVB-Q100

pastedImage_1.png

Hope this helps!

Daniel

0 Kudos

2,574 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi Daniel,

the version you have works on cut1 device (0N77P) not on cut2(0N47T). Attached is the one that works on cut2 MCU.

BR, Petr

2,574 Views
dumitru-daniel_
NXP Employee
NXP Employee

Petr, 

That's strange. I have only cut2(0N47T) and it works fine.

Best regards,
Daniel

0 Kudos

2,574 Views
PetrS
NXP TechSupport
NXP TechSupport

Daniel,

after double check, and several power down/up yours is working too. Thanks.

Anyway I have bootloader version 1.6.7.35

pastedImage_1.png

and the RBF file included works on cut1.

BR, Petr

2,574 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi Lutz,

the LPUART2 (pins PTD7/TX and PTD6/RX) is used with baudrate 115200bps.

BR, Petr

2,573 Views
koehlerl
Contributor IV

Hi Petr,

but with LPUART2 I can’t connect to the PC RappID BL Tool and the trace window is empty .

With the LPUART0 I get the trace see attachment. But it don’t works.

Regards Lutz

Von: PetrS

Gesendet: Donnerstag, 31. August 2017 10:21

An: Köhler, Lutz <lutz.koehler@acd-antriebstechnik.de>

Betreff: Re: - Re: RappID Bootloader S32K144

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: RappID Bootloader S32K144

reply from Petr Stancik<https://community.nxp.com/people/PetrS?et=watches.email.thread> in S32K - View the full discussion<https://community.nxp.com/message/938684?commentID=938684&et=watches.email.thread#comment-938684>

0 Kudos