I purchased the RD-HVBMS Bundle and installed S32K DS According to the "BMS Software Installation Guide (rev2.0)" to build the examples.
Import example code and use "Update Code" command, but there are still 5 errors.
How can I fix it?
S32K Version details are as follow image
The installation details are as follow image, It's only about SDK
Error details are as follow Image
已解决! 转到解答。
Sorry for the confusion i missed you latest screenshot showing all the installed packages, please ignore my last message.
PFB is "please find below"
As I could see that the s32xx development packages , s32k3 platform package and s32k3 platform tools package are missing in your s32ds?
I recommend you to do a fresh installation, and follow the sequence of installation of the packages mentioned in the installation guide.
Sorry for the confusion i missed you latest screenshot showing all the installed packages, please ignore my last message.
Which hvbms bundle does the customer have 400v (775,772) ,400v(774,772)?
-> RD-HVBMSCTBUN (S32K344 / MC33775A)
As the customer has opened hvbms Integration proj for 400v (775,772)....
-> The last image above shows that the project was opened but the build failed.