I purchased the RD-HVBMS Bundle and installed S32K DS According to the "BMS Software Installation Guide (rev2.0)" to build the examples.
Import example code and use "Update Code" command, but there are still 5 errors.
How can I fix it?
S32K Version details are as follow image
The installation details are as follow image, It's only about SDK
Error details are as follow Image
Solved! Go to Solution.
Sorry for the confusion i missed you latest screenshot showing all the installed packages, please ignore my last message.
Hi,
Have you installed the FS26 sbc package in s32ds?
After installation, the result is as follows.
More bugs occur and build stops midway.
As mentioned in the SW installation and user guide did follow the steps as i could see from the screenshot that some packages are missing
As mentioned, the picture above is only for the SDK. (Filter applied)
It's the same as you without any filters applied.
As mentioned above, I did Installation According to the "BMS Software Installation Guide (rev2.0)", the document you send.
and What is "PFB", Could you tell me?
PFB is "please find below"
As I could see that the s32xx development packages , s32k3 platform package and s32k3 platform tools package are missing in your s32ds?
I recommend you to do a fresh installation, and follow the sequence of installation of the packages mentioned in the installation guide.
Sorry for the confusion i missed you latest screenshot showing all the installed packages, please ignore my last message.
This was resolved once and for all with the "reimport project".
Thank you so much for your help.
Which hvbms bundle does the customer have 400v (775,772) ,400v(774,772)?
As the customer has opened hvbms Integration proj for 400v (775,772)....
Which hvbms bundle does the customer have 400v (775,772) ,400v(774,772)?
-> RD-HVBMSCTBUN (S32K344 / MC33775A)
As the customer has opened hvbms Integration proj for 400v (775,772)....
-> The last image above shows that the project was opened but the build failed.